Posted on May 14, 2017 at 10:37Hello Pawel,First of all, LoRa and Spirit1/S2-LP (Spirit1 new generation) are two completly separated technologies: ST is providing specific modules supporting LoRa communications (http://www.st.com/en/wireless-connec...
Posted on April 13, 2017 at 18:33Hello Mukhtar,Hard to have a clear view on the issue. What I would recommend is to swap some BlueNRG-1 chips from working boards with ones which are on faulty boards to see if the issue follows the board or the chip....
Posted on April 01, 2017 at 09:57Regarding the hardware part, you can have a look at the application note AN4819:http://www.st.com/content/ccc/resource/technical/document/application_note/group0/5d/e4/cf/d0/5f/30/4c/38/DM00263000/files/DM00263000.pd...
Posted on March 31, 2017 at 11:05Hi,BlueNRG-1 is a standard Cortex-M0 so it can run as a stand alone MCU.All documentations and the SDK can be found in the following link: http://www.st.com/en/wireless-connectivity/bluenrg-1.html .Regards,Julien
Posted on March 31, 2017 at 09:57 BlueNRG-1 DK is available on IAR/Keil and TrueStudio (GCC based)It is a standard cortex M0, so programming is done like on every other microcontroller. There is just a library managing the RF part.BlueNRG-GUI and t...