Hi,I have an issue with the CAN1 controller in my MCU. I have connected the CAN transceiver to PA12(TX) and PA11(RX). When connected to the CAN Bus I can see the frames coming to the MCU(RX line) and the ACK bits are visible on the TX line. Unfortuna...