User Activity

Hi, when I generate code for the SMT32L412RBTxP using TSC with CubeMX  I get duplicated entries in tsl_user.h.One channel does not work. So I edit Channel 2 to use the missing group and IO:It now works, but when code is regenerated with CubeMX it ove...
Hi, I have built an RC5 IR remote transmitter that almost works on a NUCLEO-L412RB-P, with modifications to the files found in x-cube-irremote. This unfortunately does not have an STM32L4 example.The bit I am having trouble with is the output polarit...
Hi I am getting nowhere trying to use the X Cube IRRemote package, please help.Should I expect the projects in en.x-cube-irremote\Projects\STM32G081B_EVAL to be imported into Cube IDE and run as a working example of the IR Remote functionality?The re...
Hi, I'm new to STM32. I have an STM32L4RI-DISCO board and would like to add an IR receiver and decode RC5 signals. According to AN4834, IRTIM can be used on STM32L4. I have downloaded en.x-cube-irremote.zip.Firstly it is not recognized by Cube MX.Sec...
Hi, I have an STM32F429I-DISCO1 board. I have been learning how to use it and I thought it would be good to see how the professionals do it by looking at the original firmware. I downloaded en.stsw-stm32138, which has STM32F429I-Discovery_FW-V1.0.3 i...