Hi Gabriel,Thanks for watching the ‘Stepper motor control over NFC’ video. The oscilloscope application running on ST25DV-Discovery is basically using STM32 IO interrupts to catch and measure the elapsed time between signal edges, in order to rebuild...
Hi,PWM1 control register (1x block) is located at address 0xF8, which is equal to 248 in decimal base. Any Read of 4 Bytes at block = 248 shall return the PWM1_CTRL register content, as long as it is not protected by password.The error that you get i...