Posted on November 05, 2014 at 22:04No, the boot0 pin is strapped to low and the uarts are not connected on my PCB. It would be easier to replace the whole MCU :( Do you see any problem with my code? Should it set the level back to level 0? What is ...
Posted on November 05, 2014 at 13:03
Hi
I also have the problem that I can't reset the RDP level backto level 0.
I wrote the following code that I can load in theRAM and execute to set the RDP level but it doesn't work. Can someone g...