User Activity

Hi,I'm having an issue with RTC module. getting an error due to no clock source is connected to rtc_ck:[ 3.645423] stm32_rtc 5c004000.rtc: rtc_ck is slow[ 3.749902] stm32_rtc 5c004000.rtc: Can't enter in init mode. Prescaler config failed.[ 3.756489]...
Hi,I need help to setup the DeviceTree for our custom board using STM32MP135FAE7 and TI TLV320AIC3254.I have read the Wiki about SAI and read and tried to implement SAI using these posts as reference:https://community.st.com/t5/stm32-mpus-products/st...
Hi,I have created a device tree for Marvell 88E6185 (10 port switch).Port9 of the 88E6185 is in PHY mode (MII) connected to STM32MP135F Ethernet2. MDIO lines of the Switch directl connected to Ethernet2 MDIO lines.Port0 is connected to Marvell 88E111...
We have designed 2 seperate boards, main board has STM32MP135FAE on board connected to Microchip LAN8742 via ethernet1 mac and it is working. second board is a network board and has Marvell 88E6185 switch on board. Ethernet2 mac on STM32MP135F is con...
Kudos from