Posted on October 28, 2014 at 11:20 Hello, I useSTM4F429II as LCD controller for application TFT display. My TFT works in DE mode, in the datasheet thereis no information about VSYNC, HSYNC, HBP and VBP... there are only info’s about CLK period, ...
Posted on October 19, 2014 at 19:05Hello ,I have a problem with button function on my card. I can use emWin library to display text, but I cannot display button. In place of button, there is a black block. As shown in the picture. Code: ...
Posted on October 20, 2014 at 09:35You are right. The code isn't the same for hard configuration, for example SDRAM and microcontroller.If I am configuring incorrectly SDRAM, nothing will appear. But I can't envisage other problem than SDRAM. What o...