User Activity

 tocuhgfx 4.22.1 touchgfx 4.22.1 When using GPU2D for rendering the textArea component in stm32u5a9, there is an issue with the content not being rendered, but the images are not affected. There is a problem with rendering fewer characters when using...
Can't touchgfx RGB565 images be mixed and displayed My two RGB 565 images overlap and only one can be displayed
ICNA3310 monitor does not support changing display direction. Does touchGFX support rotation,Will the rotation of touchGFX by 90 only change the height and width of communication?Will rendering data not be modified?笔记
STM32U5  + LSM6dslI want to read the general accelerometer register of the I2C interface.I think it can be achieved by using HAL_I2C_Mem_Read ().I set the second argument DevAddress to the value of the accelerometer slave address shifted left by 1 bi...
STM32CubMx 版本 6.9.1GPDMAPWM配置法典/* TIM4 初始化函数 */void MX_TIM4_Init(void){/* 用户代码以 4 开头TIM0_Init *//* 用户代码结束 TIM4_Init 0 */TIM_ClockConfigTypeDef sClockSourceConfig = {0};TIM_MasterConfigTypeDef sMasterConfig = {0};TIM_OC_InitTypeDef sConfigOC = {0};/* ...