Hello @MatasOn222
To help you with this issue, can you pleas open an online support ticket on this page https://ols.st.com/s/.
You can then post a link to it in here and i'll be able to help you with the files.
Best Regards,
Lucas
A follow up on this issue for all members.
The correct way to setup and use the FxImageCreator is the following:1- Create a temporary directory. Inside it, place both the tool's *.exe and another folder containing the web content you want to genera...
@Faust
Can you please open an online support ticket in this link so I can further assist you ? https://ols.st.com/s/
During my testing I never faced such problems, so i'd like to dig in deeper, if you don't mind. Kindly include my initials (LC) and ...
@Faust
The block size mentioned in the readme file is related to a NOR Flash standalone device. However, this parameter should be modified to match the physical block size of the Flash memory that you are using.
The Linux compatible implementation sh...
Hello @Faust
I was a contributor to this article so I will answer in B.Montanaris' place.
Here is an example command that creates a file called 'image_test.bin', with a Image size of 1MB (1048576 bytes) FileX sector size of 512 (default value for Fi...