Hello,I'd to drive two 3-phase BLDC with FOC & Hall on EVSPIN32G4-dual board, generated the code from MCSDK6.2 (support dual motor control).First, I control the M1 motor only, it's well, then stop the M1 and control the M2, it's also well.But when I ...