Posted on September 09, 2014 at 07:33Hey thanks, that fixed the problem. This is adapted from the STM32Cube_FW_F4_V1.1.0/Projects/STM32F429I-Discovery/Examples/FMC/FMC_SDRAM/Src/stm32f4xx_hal_msp.c example. It seems the documentation at the top of t...
Posted on September 06, 2014 at 21:19Hey, I'm not able to get this example to work for the amount of memory that should be available in SDRAM (8MB or 0x800000). In fact, the maximum I seem to be able to get is 2MB, adding 1 word (4 bytes) beyond tha...