Posted on September 01, 2014 at 03:30HiI need help in identifying the VIPER or any other device for a 15W and 30W LED Driver for Street Light. The input is 150V to 310V AC @ 50Hz.ThanksKiran M R
Posted on September 01, 2014 at 03:27HiI need help on designing a 12V, 1A and 12V, 2A SLA Battery Charger. The input is 150V to 270V AC @ 50Hz.This is urgently required and would appreciate any help in this regard.ThanksKiran M R