User Activity

Hello, I am working with STM32G030K8T6 microcontroller and I am using an independent watchdog (IWDG). The device goes into standby mode under certain conditions, but since I cannot turn off the IWDG, I am trying to reset the IWDG by waking up with RT...
Hello,I am developing a BLE application using the STM32WB Custom Template. In my project, I want to implement the Whitelist feature. My goal is to start the device in normal advertising mode initially, obtain the MAC address of the connected device, ...
Hello,When I add the BLE stack to the STM32WB35CEU6A, I notice that the RTC and timer settings don’t work correctly. With the BLE stack enabled, I can’t get accurate time information from the RTC and timer, or there are inconsistencies in the timing....
Hi, I want to use the Fast transfer mode on ST25DV64KC. I am using X-NUCLEO-NFC03A1 as a reader. When I write code for fast transform mode in X-NUCLEO-NFC03A1, I get an error. Do I need to make any adjustments in ST25DV64KC? Rgds KU
Hi, In this video "https://www.youtube.com/watch?v=FqCvsywsAtQ" at 3:11, the user is sending data with NFC by entering a password.As a similar process. I want to do it with st25dv64kc with X-NUCLEO-NFC03A1 for encrypted reading / encrypted writing. B...
Kudos given to