benjaminjames
Associate
since
2023-11-02
2024-01-14
User statistics
2
Posts
0
Solutions
1
Kudos given
0
Kudos received
View all badges
STMicroelectronics Community
About benjaminjames
Options
Report User
User Activity
Posts
Replies
Need help with programming STM32H563 using UART
2023-12-11
I had created a project in STM32CubeIDE for the STM32H563 chip. I was able to flash it through UART1 using STM32CubeProgrammer but the code seems not executing. The code is just to toggle a LED every 500ms int main(void) { /* USER CODE BEGIN 1 */...
Re: Need help with programming STM32H563 using UART
2023-12-11
Is there anything particular to look for while flashing the ELF file tho the chip through UART with the help of STM32CubeProgrammer.
Kudos given to
User
Count
TDK
1
View all