Posted on July 14, 2015 at 06:58 Hi Mehmood, I believe that the folks of Stlink utility, simply forgot to add the proper flash loader to v 3.6. The AIR IDE has its own flash loader but it is unstable. For some reason loading 14MB of graphics d...
Posted on July 10, 2015 at 07:06Hi Mehmood, Thanks for the tip, I tried the N25Q256A-STM32469I-EVAL in STLINK utility with STM32746G-DISCO_Demo_V1.0.1.hex, it programs the internal flash no problem when it is trying to program the external NOR...
Posted on July 04, 2015 at 20:15Hi guys, OK the readme.txt says in the demonstration folder to load the binary original firmware (STM32746G-DISCO_Demo_V1.0.1.hex): - Open STM32 ST-Link Utility V3.6, click on ''External Loader'' from the bar menu t...