Hello @KarthikGo,
I apologize for the delayed response.
I have successfully connected an STM32WL33 using the ST-Link V2 with version 2.19.0 of STM32CubeProgrammer.
Could you please try again using this version? You can download it from the followi...
Hello @MarekK ,
For high flash sizes, the DBANK bit is always set to 1, so it was decided to remove it from the Option Bytes tab since it is not configurable. For lower flash sizes, the DBANK bit remains visible and configurable. Please refer to Ta...
Hello @Aurel ,
Thank you for your feedback.
I'm glad to know that programming is now working for you.
The issue you encountered is related to a known problem within CubeProgrammer when the DBANK is set to 0 (incorrectly assumes a sector size of 16K...
Hello @Rafa096 and welcome to the Community,
Unfortunately, there is no way to modify the Data_Base path within the STM32CubeProgrammer API at this time. This feature has already been requested from the STM32CubeProgrammer development team.
Interna...