Posted on July 05, 2017 at 21:18Hi CliveI need your help. In the previous example it works correctly, but for it to work I have to put a breakpoint in my debugger, and then continue. No debugger no ST-Link does not work. Do not start DMA.Thanks in a...
Posted on August 10, 2016 at 11:03HelloIs possible, to config ADC1, ADC2 and ADC3 of mode independent?i.e. ADC3, in mode scan whith DMA PA0, PA1, PA2 and PA3. resolution 8bits.ADC1 in mode independent. for canals 16,17 and 18. request information ...
Posted on March 26, 2015 at 07:46No works well .. Maybe I did not understand the steps.It is a commentary on the double buffer based on a RAPID reading. I have not implemntado. I seemed at first code more flexible to change.
Posted on March 25, 2015 at 14:45Definitely after reading about double buffer I think is the solution. Could you tell me the steps to configure the program in this way?
Posted on March 25, 2015 at 08:09I really need something more robust. Sometime I would put more shots on the table and would return to having to touch this code. I thought this would have more defined micro utilities for these tasks.Posivilidad you...