User Activity

Hello,This is an interesting problem. We are developing a system. Touchgfx task are independent from main task. It is hard to explain all software but i will try to make it simple.There is only one screen in touchgfx project and it is startup screen....
Posted on August 07, 2014 at 09:58Hello,when i call BUTTON_SetText() hard fault error occured. What is the possible reason? I can create button. I can write messages on screen but i cannot set button name.  #stemwin #stemwin
Posted on August 06, 2014 at 11:49Hello, I have a problem for driving LCD. Let me tell you about hardware first:- I am using STM32F427VI, - I am using FMC for communicating. D0..D15 and A16 and NE1 pins.- Pin connections made for 8080 mode.- I am no...