I tried also the process to add the libmodbus : libmodbus add to weston image.in conf/local.confIMAGE_INSTALL_append += "libmodbus"bitbake st-image-weston==> result package/tmp-glibc/deploy/deb/cortexa7t2hf-neon-vfpv4/libmodbus5_3.1.6-r0.0_armhf.deb/...
Hi @FHami.1 You can use the STM32CubeProgrammer to create a new partition, for example in .tsv file add " P 0x14 rootfs2 FileSystem mmc0 0xA5484400 st-image-weston-openstlinux-weston-stm32mp1.ext4.Then you need to update in /boot/mmc0_linux/stm32mp...
hi @zqizh.1 Note the integration the AWS greengrass has been validated with the openstlinux MMDV2.0.0.But according to your build error you can try to delete this dependency ==> python3targetconfig in .../layers/meta-virtualization/recipes-extended...