"Solved"This seems to be related to my USB connection on MacOS (M1).Using a hub/converter from USB-C to USB and connecting to the Nucleo using a USB-USBmicro cable. When I start the ST-Link fw updater the red light blinks a while (showing that data t...
I have NUCLEO-U575ZI-Q with board MB1549C.With -d8_d32_msc_br I get The specified firmware type does not match the detected one: can not update.(Seems the parameter is for certain Nucleo type)Without it, the upgrade tries to upgrade the firmware to t...