Posted on July 24, 2014 at 09:31Dear Mr Marco,yes the motor DC connected to L9958 outputI use Microcontroller 16 bit(with SPI 16 bit) for control L9958,send command for rotated left nd right is ok,but when comunicated via SPI how to know if our conf...
Posted on July 11, 2014 at 09:47I am developing pcb motor controller used IC L9958,the questions are;1.the first answer after power on reset is IC identifier =fsi bit =00000110...?2.for configuration register (CFG_REG) I send 0b00XX1011XXXX111X ;......