User Activity

Porting SBSFU 2.6.2 to STM32G0B1CEU6 (512K FLASH and 144K RAM) based on Nucleo-G071RB example.See the history of my previous Solved: SBSFU 2.6.2 firmware swapping issue - STMicroelectronics CommunityAfter I solved the firmware swapping issue, I went ...
Hi Guys,Ported SBSFU 2.6.2 to STM32G0B1CEU6 (512K FLASH and 64K RAM) based on Nucleo-G071RB example.Modified mapping_fwimg.ld as below: /* Slots must be aligned on 2048 bytes (0x800) */ /* swap (4 kbytes) */ __ICFEDIT_SWAP_start__ = 0x0804...
Kudos from