User Activity

Hello, I hope you are doing well.I’ve developed a product using the STM32H573I-DK kit as a reference and the MXCHIP EMW3080 Wi-Fi module. We decided to design our new hardware in such a way that the Wi-Fi module could be connected just like in the de...
Hello, I hope you are doing well!I developed a project based on the STM32H573I-DK example with TrustZone. However, in the final board, I am using the STM32H573VI microcontroller. I migrated all the code to this microcontroller, made the necessary pin...
Hello, I hope you are well.I'm working with a project, where the base code is the example "STM32CubeExpansion_Cloud_AWS_H5_V1.0.0", I need the current time somehow. So I thought about SNTP, however, I don't have much knowledge on the subject, I would...
Hello everyone, I hope you are well.I'm working on a project and one of the requirements is connection to AWS, so I chose to start with the STM32H573I-DK kit, where following the "STM32CubeExpansion_Cloud_AWS_H5_V1.0.0" step by step I managed to conn...
I'm working with the stm32h573i-dk kit and I need a connection to AWS. I performed the step-by-step procedure as described in the webinar https://content.st.com/stm32h5-connects-smart-things-in-a-secure-way.html, however, I got stuck at the end, wher...