Hi,One possible reason could be that the BLE stack is preventing the MCU from entering Standby mode. The BLE stack might be running on the CPU2 and if it's not properly put into a low-power state, it can prevent the system from entering Standby mode....
Hi,Flashing an STM32 system image to a Raspberry Pi board SD card using the STM32CubeProgrammer is not directly possible. The STM32CubeProgrammer is designed to program STM32 microcontroller devices, not Raspberry Pi boards. However, you can use the ...
Hi,Yes, it is possible to implement secure boot without using TrustZone for STM32U585. The STM32U585 microcontroller supports a range of security features including Boot lock, OTP, and secure address space which can be used to implement secure boot.T...
Hi,The DTCM is a high-speed memory that is directly connected to the processor and is not directly accessible by the DMA controller. The DTCM is intended for storing critical real-time data and code that requires low-latency access. The DMA controlle...
HiThe specific field descriptions for the $PSTMTTFF message are not directly provided in the ST Teseo III binary image - User manual (UM2399 Rev 4). It's possible that the fields in your output message represent various TTFF measurements under differ...