Based on the STM32U5 series reference manual, the SAI peripheral cannot stay on during STOP modes. This is because the SAI peripheral is clocked from the APB clock, which is gated (turned off) during STOP mode to save power.As for the MDF/ADF periphe...
Based on the information provided, it seems you are trying to use the pcsc-lite driver with the ST25R NFC reader on a system running on STM32MP1. While the ST25R series does support various host interfaces including SPI and UART, there isn't a direct...
The VL53L5CX sensor uses target status codes to provide information about the status of a target. These codes range from 0 to 13 and 255, as described in UM2884-Rev 3, chapter 5.5 Results interpretation, table 4. Each code provides a short descriptio...
Based on the error message you're seeing, it seems like there might be an issue with the STM32CubeProgrammer. Here are a few steps you can try to resolve this:Check your proxy settings. You can do this in STM32CubeIDE by going to Window -> Preference...
Based on your description, it seems like you're on the right track with your approach to integrating the analog magnetic sensor into your MCSDK 6.1.2 generated project. Modifying the hall_speed_pos_fdbk.c and hall_speed_pos_fdbk.h files to provide an...