User Activity

Hi,STM32U5A5VJT6Q has 2 VDD11 pins. Should these be connected together using an external trace on a PCB? I did look at Nucleo U5A5ZJ-Q schematic but I'm still not sure.Thanks,Adam
Hi,I want to buy LDL212PUR LDO. I have 2 questions:1. Can it work reliably with ceramic capacitors?2. What are the recommended resistor values for voltage adjust version?I cannot find this information in the datasheet.Thanks,Adam
HiI'm trying to connect an SD card to my Nucleo U5A5ZJ-Q board using SDMMC peripheral and use it with FatFS library. When I use 1GB card and 4 bit mode, everything works fine. By "works fine" I mean that:1. it passes this FatFS test: http://elm-chan....
Hi,I recently started exploring what STM32WL MCUs offer but I don't really understand a few things yet:1. I read somewhere that these STMs are based on SX126x LoRa radio. Is that the case?2. If so, does enabling "SUBGHZ_PHY" in middlewares in CubeIDE...
Kudos given to