User Activity

Hi there,   I read this document and it mentioned that the function "vl53l8cx_set_VHV_repeat_count" can be used to compensate for the ranging error caused by temperature. I would like to know the principle of VHV calibration compensation. Is it relat...
I want to know whether the calculation of integration time using kcps and signal peak count is correct or not Signal = 3.83 kcps/spad (3.83*1000*211(SPAD ea ))/2099  =385    =>  1/385 = 2.6 ms Ambient & signal kcps, is the integration time the same?...