User Activity

Hello everyone,I am experiencing a fairly impactful problem with STOP3 mode in a FreeRTOS application that runs in a STM32U585VIT6Q.The system has this behavior: it wakes up, performs operations on SPI3, write some informations on internal FLASH, ret...
Hello everyone,I'm working on a STM32U585 application which works on STOP3 mode and on a customized electric circuit. One of the wake up sources is the ST25's GPO which should generate a pulse when a message is sent via FTM when mailbox is enabled. I...
Hello everyone.I have an application that is based on FreeRTOS and works in power saving mode with STOP3 mode. I have configured each WakeUp pin and all the necessary arrangements for the entrance and exit from low power mode. However, so far I've ex...
Hello everyone,before introducing you to the issue I am experiencing, let me share my setup:uC: STM32U585I2C: Fast Mode PlusIde: STM32CubeIdePower Source: 3.6VDC (laboratory power supply)st25dvxxkc package: GitHub st25dvxxkc RF Reader: ST25 App (Goog...
Hello,i'm experiencing issues on M24SR64-Y chip. In fact, i can't write any record neither via RF or I2C. Until this morning (for weeks, actually) i was working fine, capable of writing whatever record i wanted to either via RF and I2C. Suddenly, it ...
Kudos given to