Hello DMeie.2,Currently ADC reference voltage is fixed to 3.3V regardless the settings in your board description. The quickest work around to avoid ADC_REFERENCE_VOLTAGE modification after each cubeMX generation is :- open the *.ioc file in your proj...
Hello JLC,According to the material you sent and your comments, it seems you reached the maximum current set in your project, therefore the current controller will not go beyond that limit. I suppose you have a propeller mounted on your motor, then h...
Hello DMeie.2,Yes you are right, sorry for the inconvenience.As a workaround, I would suggest to create a project with a positive gain and save the following values:- In Speed Sensing config panel->Observer and PLL: G2 gain (if you are in sensorless ...
Hello DMeie.2 Yes it could be an issue, you may need to set a negative gain for the current sensing which is supported in MCSDK 6.2.1 version. Best regards