Hi E-John,Yes I can launch UG. There was a message to update the UG version to 9.15.0.0, which I did. No messages related to the firmware (which is indicated to be version V3.18.9)..We work in Octave. We can now get data from all settings except thos...
Hi FedericaIs V3.18.9 the latest firmware for the STEVAL-MKI109V3 ?We have updated the Unico Gui version from 9.14.6.0 to 9.15.0.0 and the motherboard does not seem to work properly - not even after returning to 9.14.6...We work with the MKI197V1 ada...