User Activity

Hii,I am using STM32H745XIX6 microcontroller for our custom boards and also enabling the Touch GFX in it, we are doing dual core debugging, and the both the cores got activated and working fine after changing some settings in debug configurations of ...
Hello,We are using STM32H745XIH6 Microcontroller for our designed custom boards. We have designed two boards named controller card (i.e. with the mentioned microcontroller mounted) and the other Power supply card.The I2C signals are generating from t...
Hi,I had 8-Gigabyte External EMMC Memory to store the images in my custom Board, as my internal flash for the STM32H745XiH6 microcontroller is only 2MB. How to store the images in the external flash (EMMC)? Should I need to change the linker scripts ...
Hi,I am using STM32H7S78-DK Board, as size of the internal Flash and Internal Ram memories are very less, I have added external flash memory and the address in the linker file of the Application mode. I also enabled XSPI2 and External Memory Manager ...
Hi,I am using STM32H7S78-DK Board, I am configuring XSPI2 in Stm32CubeMX for enabling external 1-Gbit Nor flash memory. But when I am writing the data into the Memory address (i.e. 0x700000000) it is going into the hard fault handler in STM32CubeIDE....
Kudos from