Dear Ladies and Gentlemen,
for you it is your daily business - for me as customer a contemporary challenge:
Something went wrong with my pin-configuration.
I measure ~1,7 V as GPIO-output of Port A instead of wished >=3.3 V.
My power supply is a ...
I work with a 64 bit linux and a stm32f411ceu microcontroller.Unfortunately there is no detection under linux from the uart port. Are there experiences or sources?
(1) Are there any experience for a data exchange via bluetooth between two STM32WB1MMC-parts?
(2) How can I use a STM32WB1MMC together with a STM32F411 board?
Are there any experiences?
(3) How can I create a data exchange between two STM32WB1MMC?
(4...
Good Evening Ladies and Gentlemen, A short introducing purpose of mine: int main(void)
{
RCC->AHB1ENR |= 0xFC; // ---> Here I would like to open the Port clock
RCC->APB1ENR |= 0xFC; // ---> Here I would like to open the USART2...
Ok - in common I think, that my control voltage is too low. The motor sounds in this way. In look to the USB voltage, there is no possibility to get this voltage per software?
F U I & ((A)nswer) - my emailaddress is ... xxx Could you send me this answer in a more common way in german language again? Thank's a lot ... sou sou sou - spoken in my time ... I would like to go on OPTO with an open common PIN as input voltage......