User Activity

Hi All,I have a 50MHz clock with 1Vpp and the MAC is not working. The only information I have from the RM and datasheet is this is a digital input pin and never mentioned about the voltage level. Please help what is the clock pulse VPP for RMII refer...
Hi All,I have a custom board with STM32735VGT(this mcu is with 1=quad SPI but using the register octpspi). I am using the micro mt25qL128 NOR flash.I am using the 1-1-1(1 bit instruction, 1 but data) for read and configure the registers, eraseI am us...