I have successfully re-built fp-cld-aws1 using STM32CubeIDE 1.8.0.I have run STEVAL-STWINKT1/Applications/BootLoader_STSAFE/STSAFE_Provisioning/Binary/Provisioning.bin, but I have not seen the following: ---------------------------------------------...
JocelynTo narrow things down further, the target platform is STEVAL-STWINKT1B with STEVAL-STWINFV1. We also have STEVAL-STMODLTE.Thanks for your help,Geoff
Hello JocelynIs there a pre-release of the IDE which fixes the problem with the secure engine/compiler problem? It is important for our project that the STM32Cube AWS Cloud function pack for STWINKT1B AWSdemo example does build with the IDE release t...