User Activity

Hi,I´m trying to get a STM32H747 Discovery board together with USB Host to operate at 1.8V VDD.At 3.3V VDD_MCU USB is working fine!What I´ve done:1. Removed jumper on JP3 and supplied VDD_MCU with 1.8V.2. Removed SB10 and supplied VDD33USB with 3.3V....
Hi,I have a bit of a problem.Currently I´m using the M7 to do all the work, it initializes all the peripherals it needs.The M4 waits for M7 to configure stuff and then goto standby mode.The problem is related to sleep/stop/standby mode of the differe...
Hi,I´ve done a lot of reading and testing...For some reason, its stated in both the datasheet and the DCMI application note that 24 bit per pixel formats are not supported. Trying to understand why...The DCMI is "stupid" in the sense that we only tel...
Kudos from