In all ST devkit code, the commandaci_hal_set_tx_power_level(0,25)is used, but changing the parameters has no effect on the transmit power (is always about 0dBm).
In a non-encrypted BLE link, the device falls back to the level of minimum power consumption (STOP_NOTIMER) between connection events. In an "LE Secure" link, the CPU is kept active. Why, and what to do about that?