Here are some addition measurements which we have done. Hardware-setup was the same.Only the chips are changed between this measurements.Labeled with 120Labeled with 940
Hi Eleon,we face the problem that the output data rate (ODR) of different product batches differs significantly. Batches with the mark 940 are close to a sampling rate of 6600Hz. And Batches with the mark120 are close to 7000Hz.Do you have any inform...
Signal bandwith is smaller than 2400Hz why would you look for frequency like 8000Hz? I good filter is a fast solution. But we faced simmilar problems, you get this kind of peaks if you don't sample with exact ODR, ODR/2 or ODR/4. Keep searching for ...