User Activity

I want to be getting my characters , including the first one from uart at 115200 baud rate and use UART to wake up from sleep, how do I do this ? The sleep mode and low power sleep mode, with all gpios changed to analog no pull and all other peripher...
I went through the examples on the ST site which have the direct implementations (not using CubeIDE generated code HAL for GPIO, SystemClock, ... config implementation)https://github.com/STMicroelectronics/STM32CubeL0/blob/master/Projects/NUCLEO-L053...
I want to listen to UART (using receive interrupt) at a baud rate of 115200 while in stop mode and retain the received characters (which are stored in a buffer) after I wake up from STOP mode using the RTC. Is that possible?If so, how do I implement ...
I went through the examples on the ST site which have the direct implementations (not using CubeIDE generated code HAL for GPIO, SystemClock, ... config implementation)https://github.com/STMicroelectronics/STM32CubeL0/blob/master/Projects/NUCLEO-L053...
HiI am able to erase two pages (my array is length 256 ), now I want to write my array to a particular memory location.Here set is the address which is 0x080E0000p_source is my uint16_t array which I want to write to flash. And length is 256.How do I...