Hi,i try to use a ADM DMA with the board in object.I generate the code with CUBE MX and i add only the function HAL_ADC_Start_DMA(&hadc1, (uint32_t*)&buff, 1); before the while loop in the main.After i start the ADC, the hadc1.State remains in HAL_A...