User Activity

Hi All,we tried to migrate from VL53L1CX to VL53L4CD for better precision in short range.both use ULD driver, we expect they work in similar way however it seems not.we set both to TB20 and compare power consumption in single shot case. It seems VL53...
Hi All,I use STHS34PF80 for presence detection with embedded algorithm however it easily get stuck in presence status and cannot release from the status.Use case:People sit in from of the sensor around 30 cm, with lens on STHs34PF80.When people enter...
Hi All,I want to port VL53L4CX bare driver to my M0+ MCU (36KB SRAM) however it cannot fit into RAM (.bss)What's RAM requirement of VL53L4CX bare driver ?(I used VL53L1CX ULD and VL53L4CD ULD driver that's ok) or how to trim down the memory requireme...
Hi All,I started with example to make STHS34PF80 presence detection working.Now I tried to add effective presence detection range.Where should I start ? Is there a suggested process ?  
Hi All,I need a mechanism to detect motionless for 10s to make device enter power saving mode.For lis2dh12, I can use HPF with low x,y,z threshold and duration to detect an event that motionless for 10s.However I need more low power accelerometer lis...
Kudos from
Kudos given to