The error message you are seeing indicates that your TouchGFX project is using more RAM and Flash memory than your STM32F746ZG microcontroller has available. To resolve this issue, you can try the following:Increase the amount of RAM and Flash memory...
Yes, there are many alternative development boards to Nucleo that you can use for your projects. Some popular alternatives include:Arduino: Arduino is a popular open-source electronics platform that is widely used for DIY projects. It has a large com...
To handle click and drag events in a custom container within another custom container, you can implement event listeners on the child container that captures the event and performs the desired action.Here are the basic steps to implement this:Add eve...