DGian.1
Associate
since
2020-01-30
2023-06-14
User statistics
3
Posts
0
Solutions
0
Kudos given
0
Kudos received
STMicroelectronics Community
About DGian.1
Options
Report User
User Activity
Posts
Replies
The raw data for the embedded internal reference voltage is measured at 30°C +/-5°C. What is the VREFINT_CAL range when the same MCU is measured at ST at 25°C and at 35°C?
2021-11-08
STM32L151xE
In the datasheet for the STM32L151 is missing the value of the sampling switch resistance R_ADC in table 55. Does anybody knows the R_ADC value?
2020-08-12
Re: In the datasheet for the STM32L151 is missing the value of the sampling switch resistance R_ADC in table 55. Does anybody knows the R_ADC value?
2020-08-12
Yes, I'm looking the internal resistance value of the MUX switch (R_ADC not R_AIN). But I also assume it is 6kOhm as in the datasheet of STM32F405.