Hi - has there been had any further development on this?Requirements are quite straightforward, I think: use external power when USB is not used, still make the internal ST-Link usable when USB is connected.So, I wonder if a permanent - and efficient...
Hi all, I know it'a bit old, but I'm facing exactly the same problem here, with a L432KC Nucleo-32 board: when powered through the +5V (CN4 pin 4), the board won't boot up. Ok, I've seen a few suggestions here, to solve this problem: 1) close (on) SB...