I just responded in another thread As far as i am aware ST updated their FUS a few months ago and the new code cannot be put on devices with an older FUS. We had to destroy a number of boards due to thisMaybe this helps.
As far as i am aware ST updated their FUS a few months ago and the new code cannot be put on devices with an older FUS. We had to destroy a number of boards due to this
You basically have to do this yourself.You will need to allocate a section of flash for your second image, create a boot-loader to download the image to the second bank and then reboot and run the second image or copy the image over after successful ...
There are a large number of fixes to this codebase since ST grabbed the source from Github, with some pretty major fixes included.I would have understood that a rebase would have been critical path for ST considering it would have reasonable affect t...
It feels like the retry code on the WB M0 is not sufficient.When dealing with multiple devices on a network, the WB M0 drops packets without sending them.Current tests ( although this is a black box) indicate that the Packet has been Queued, however ...