AMaha.1
Associate
since
2020-01-21
2023-06-14
User statistics
2
Posts
0
Solutions
0
Kudos given
0
Kudos received
STMicroelectronics Community
About AMaha.1
Options
Report User
User Activity
Posts
Replies
I'm using STM32F030K6T6TR and i'm trying to use the flash memory. It worked to erase the pages that i need but when i write i get a hard fault error
2020-01-21
#define FLASH_USER_START_ADDR 0x0800FC00UL#define FLASH_USER_END_ADDR 0x08010000UL uint32_t Address = 0, PageError = 0; __IO uint32_t data32 = 0 , MemoryProgramStatus = 0; /*Variable used for Erase procedure*/ static FLASH_EraseInitTypeDef Era...
Re: I'm using STM32F030K6T6TR and i'm trying to use the flash memory. It worked to erase the pages that i need but when i write i get a hard fault error
2020-01-21
Yes i wanted to try the FLASH_TYPEPROGRAM_DOUBLEWORD but i forgot to put the FLASH_TYPEPROGRAM_WORD back. It's still not working with the other options