Hi Remy, thanks for your reply.yes it is restarted.this part is generated by the ioc. it's not part of the user code.I found out that, if I use the exiting project(which is setup using stm32cubemx version6.6.0 with STM32Cube FW_WB V1.14.1) and migrat...
Hi, I am facing the same problem.I had my user board working orderly with 1.13 and after migrating to 1.15, it couldn't be connected at all, and the toolbox will popup a msg saying error occurred during connecting. I tried to rebuild a new project us...
Hi everyone,i am using STM32WB5MMG to test ble features. stm32cubemx version6.7.0 with STM32Cube FW_WB V1.15.0coprocessor binaries version stm32wb5x_BLE_Stack_full_fw.bin V1.15.0 / 05-Nov-2022after I setup everything following the video and flash in ...