Thanks Imen,Note also that the description will be improved a bit in the next version of RM0456 (see below).And in practice, nothing to do on user side from a firmware standpoint. Any Flash page can be cycled up to 100 000 times provided that this is...
Hello Alasa995this may be due to a slow internet connection. Please try again at an other time.Otherwise , please share an Email address so we can provide the expansion package.Best regards,Stéphane
the XCUBE-EEPROM software is designed to work with the MCU internal Flash. It has to be adapted for the external Flash characteristics (Flash line size, Flash page size...).
Hello Manto,could you please tell us if this issue is systematic or happens only on some devices.Which STM32 (or board are you using ?)Best regards,Stéphane