I want to use the STEVAL-SPIN3202, but the max voltage is 6.7 V to 45 V.Can't I use 48V as the max voltage? my motor is rated at 48V.I saw that the STD140N6F7 which is incorporated in the design is 60V...thanks
Yes but why? did you look at the schematic? I did, and I saw no reason to use 48V. I would like to get an answer which is based on the schematic.Thanks.