Board Details:MCU: STM32G431RBPWM : 6PWM (complementary) Current Sensing: 2 Isolated hall sensors on Phase U and V (inline)Motor Rating : Internal PMSM , 60V , 5KW , Nominal Current 100Amp
I guess I have to start with MCSDK 5.4.8.It has custom board support.There is one more version MCSDK 5.Y.4 It too have custom board support.But after generating the code , its not able to communicate with Motor Pilot of 5.Y.4.Same configuration works...