User Activity

 Hi Team i designed the schematic shown below for my automotive GPS Tracker Screenshot 2024-05-27 1500131355×883 62.2 KBHere i used diodes for droping the voltage main regulator D17 used for 5 to 3.8v approx.auto bat circuit D7 used as 4 - 3.8v appro...
Hi Team,I am currently working with the STM32G0B1CET6 microcontroller and using two Abracon crystal parts, ABL-8.000MHZ-B2 and AB38T-32.768KHZ-B. However, I am encountering issues with the crystal when I use heavy ( like code more than 50% ram & flas...
Hi Team , I'm using your ST acc and gyro LSM6DSOTR datasheet https://www.st.com/resource/en/datasheet/lsm6dso.pdf at sometime an acc stop sending its values can you guys please help me figure the issue  and whenever i restart then its sending values ...
I have attached the schematic actually trying to replace the mcp73831 so mayI program stm32 to connect or disconnect using MOSFET to charge or control my lipo battery if its rating its 0.7C, or you can say approx we need to charge 500mah with or...
I simply mean that how I can test and verify all the sections of my PCB like here I'm sharing PCB Schametic power section because main section is power section so let us know what things I should keep in mind and so on,so main agenda is that here is ...